Write/Read |
About Pulse Measurements |
Description |
In Narrowband pulse mode, choose to set the Pulse Repetition Frequency automatically or manually. This is labeled "Optimize Pulse Frequency" on the user-interface. To make changes manually, use MasterFrequency Property or MasterPeriod Property. |
VB Syntax |
pulseMeas.AutoOptimizePRF = bool |
Variable |
(Type) - Description |
|
pulseMeas |
A PulseMeasurementControl (object) |
|
bool |
False - Manually set the PRF for the measurement. True - Automatically set the PRF for the measurement. |
Return Type |
Boolean |
Default |
True |
Examples |
pulse.AutoOptimizePRF = True 'Write |
|
value = pulse.AutoOptimizePRF 'Read |
|
C++ Syntax |
HRESULT get_AutoOptimizePRF(VARIANT_BOOL *pVal); HRESULT put_AutoOptimizePRF(VARIANT_BOOL newVal); |
Interface |
IPulseMeasurementControl |