The Pulse Setup dialogs shown in this topic are now integrated in the VNA firmware and are available with S9x026A/B.
Note: For information about pulsed measurements using a PNA-X, refer to Active-Device Characterization in Pulsed Operation Using the PNA-X.
External pulse generators can be used along with the VNA internal pulse generators. Learn more.
See Swept IMD note regarding IF Filter setting
App Note: Active-Device Characterization in Pulsed Operation Using the PNA-X (1408-21)
How to start the Pulse Setup dialog |
|
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
|
The appearance of this dialog changes slightly between two pulse measurement types: Standard Pulse and Pulse Profile, as shown below. Additionally, the dialog can be switched between Basic and Advanced modes. The dialog comprises four groups of properties for pulse configuration: Standard Pulse (PNA/PNA-X)
Standard Pulse (PNA-X Pro)
Pulse Profile (PNA/PNA-X)
Pulse Profile (PNA-X Pro)
Basic and Advanced ModesBasic mode settings appear when you first open the dialog. Clicking the Advanced >> toggle button expands the dialog to access additional pulse settings. Click Basic << to hide the advanced settings. Basic mode controls simple pulse measurements, using the default (auto-selected) settings in the Advanced section of the dialog. Advanced mode accesses the additional settings, providing you maximum control of a pulse measurement configuration. Pulsed Profile measurements are performed in a Standard channel. (See Measurement Class.) Standard Pulse measurements are supported by most channel types. Several VNA measurement settings are controlled by Pulse Setup, such as sweep type, number of points, and so forth.. Pulse MeasurementEnable Pulse (checkbox)When enabled, the source and receivers are pulsed. The default state is disabled (not checkmarked). The Standard Pulse and Pulse Profile radio buttons remain selectable in either state. Standard Pulse (radio button)This measurement type is selected by default. With pulsed RF, the VNA can be configured to sweep in frequency, power sweep, and CW time. This measurement type is used for Point-in-Pulse measurements and Pulse-to-Pulse measurements. Pulse Profile (radio button)Pulse profile measurements provide a time-domain (CW frequency) view of the pulse envelope. Profiling is performed using a measurement technique that "walks" a narrow receiver "snapshot" across the width of the pulse. This is analogous to using a camera to take many small snapshots of a wide image, then piecing them together to form a single, panoramic view.
Pulse Profile measurement using default settings and R1 receiver.
Pulse TimingPulse WidthDefines the width of the RF pulse. See measurement timing to learn how to control the receiver width and delay. In Advanced mode (expanded), the label "Pulse Width" will include an asterisk *. This value is linked to the pulse width of the modulating source, which will also be indicated with an asterisk * in the timing table. Pulse PeriodDefines the period (i.e. one complete pulse) of the pulse train. Pulse Frequency (PFR)The reciprocal of Period (1/ Period). See Internal Pulse Generators to learn more. PropertiesDetectionAuto is enabled by default. Check to automatically switch between Narrowband and Wideband based on the Pulse Width. Unchecking the Auto checkbox will allow the detection method to be manually specified through the dropdown menu. For Standard Pulse: PNA/PNA-X models: The VNA will select Wideband any time the RF pulse width is longer than the shortest receiver acquisition time, which is approximately the reciprocal of the widest available IFBW with some added margin. For RF pulses narrower, the VNA selects the Narrowband measurement mode. PNA-X Pro models: The VNA will select Wideband for RF pulse widths >= 100ns and Narrowband for narrower RF pulse widths. For Pulse Profile: PNA/PNA-X models: The VNA will select Wideband any time the RF pulse width is longer than the shortest receiver acquisition time multiplied by 6, which is approximately the reciprocal of the widest available IFBW multiplied by 6. For RF pulses narrower, the VNA selects the Narrowband measurement mode. PNA-X Pro models: The VNA will select Wideband for RF pulse widths >= 600ns and Narrowband for narrower RF pulse widths. IF PathAuto is Enabled by default. To manually change the IF Path settings, uncheck the Auto checkbox and click the "IF Path..." button to open the IF Path dialog. IFBWAuto is Enabled by default. When Auto is enabled in Standard Pulse mode:
When Auto is enabled in Profile Pulse mode:
Point CountDisplays the read-only point count that will be set when the settings are applied. X-Axis Start/StopThis property is only available in Pulse Profile mode. Auto is Enabled by default. If Auto is selected, the VNA will automatically change the X-axis start and stop times so that the profile is centered on the screen and occupies 50% of the screen. If Auto is not selected, the start and stop times may be manually specified. Note: The X-Axis timing values are affected by the "Rcvr ADC Delay" and "Nominal RF Mod Delay" values. SW Gating for Narrowband (N522xB PNA and N524xB PNA-X models only)This property is only available in narrowband detection mode. When checked, all data outside the measurement band is zeroed. This improves sensitivity. Display True Power for Narrowband (NA520xA PNA-X Pro models only)This property is only available in narrowband detection mode. Enabled by default. Enabling this checkbox will display the true RF pulse amplitude rather than the average power calculated over the pulse duty cycle. Note: When driving the IF gates with external pulse generators, the IF gate width must be set in the Measurement Timing table for the VNA to determine the correct output power. Optimize Pulse Freq for NarrowbandThis property is only available in Narrowband detection mode. Enabled by default. When disabled the VNA may modify the specified Pulse Frequency by a small amount to produce a better measurement. When enabled the VNA may modify the specified Pulse Frequency by a larger amount to produce a better measurement. Measurement TimingTable PropertiesSource (Rows)These rows control the modulators associated with each source or source port. Source rows whose names contain an asterisk * have width values that are coupled to the Pulse Width property in the Pulse Timing panel. Recv (Rows)In Wideband detection mode these rows control the receiver timing. The receivers can only be driven by Pulse0. In Narrowband detection mode these rows control the IF gate timings, which can be driven by any pulse generator other than Pulse0. Width and Delay (Columns)Auto is enabled by default. When Auto is enabled, the widths and delays will be automatically chosen by the VNA. In Standard Pulse mode:
To manually change the widths or delays, uncheck the Auto checkbox to enable the cells in these columns. Pulse Gen (Column)Auto is enabled by default. While Auto is enabled the VNA will select Pulse1 to drive all source modulators and Pulse2 to drive all IF gates. To manually specify which pulse generator drives each row, uncheck the Auto checkbox to enable the cells of this column. In addition to the internal pulse generators, other pulse generator selections are available:
TriggerNote: This provides the same selections as provided in the Pulse Generators Setup dialog and the Trigger dialog on its "Pulse Trigger" tab. This combo box allows you to select the pulse trigger source. Choices include the following:
Offset Pulse Delays Using (checkbox)This checkbox is also found in the Pulse Generators Setup dialog. Disabled by default. When enabled, the Nominal RF Mode Delay and Rcvr ADC Delay may be subtracted from the delay values displayed. The delay terms compensated for in this subtraction depends on the position of the element in the signal processing chain that this pulse generator is driving. For example, pulse generators driving modulators have no delay subtracted, but a pulse generator driving ADC triggering (Pulse0) will have the Nominal RF Mode Delay and Rcvr ADC Delay subtracted from its delay. Modulator DelayThis is the approximate delay of the RF modulator. This value is always active and may be changed as needed. If "Auto Width and Delay" is enabled, this will be used to automatically set the delay. If "Offset Pulse Delays Using" is enabled, this will be used to offset the delay values in the table. In Narrowband Detection mode, this value is used to offset the X-axis timing. ADC Delay(Not shown on NA520xA PNA-X Pro models.) This is the delay of the receiver ADCs. This value is fixed and cannot be changed. If "Auto Width and Delay" is enabled, this will be used to automatically set the delay. If "Offset Pulse Delays Using" is enabled, this will be used to offset the delay values in the table. In Narrowband Detection mode, this value is used to offset the X-axis timing of pulse profile measurements. Pulse Generators... (button)This button is only available if Pulse is enabled. Opens the Pulse Generators Setup dialog. Plot Pulse Timing... (button)This button is only available if Pulse is enabled. Accesses the Pulse Timing dialog with an interactive screen, displaying pulse characteristics in the time domain. Plot Pulse is disabled for all narrowband pulse measurements. This dialog is accessed from both the Pulse Setup and Pulse Generators Setup dialogs. Right-click on the display area to access the menu selections described below:
Autoscale - Automatically scales the data to fit vertically within the display grid area. Display marker annotation - Select to display marker annotation in the top-right of the display. Show graticule - Select to display the graticule. Add marker to: - Select to add a marker to a displayed pulse trace. When a selection is made, the mouse pointer changes to a "+". Click in the display area and the marker will appear. Drag the marker to the desired position. Each time this selection is made, a new marker will be added. Copy to Clipboard - Copies a bitmap of the trace control (Display) to the clipboard. It can then be pasted into any document that accepts bitmaps. Print... - Prints the displayed data. Scale properties... - Accesses the Scale Properties dialog: Stimulus - Sets the Begin and End displayed on the X-axis in seconds. Response - Sets the Reference level in the center of the Y-axis and sets the scale per division.
|
|
Note: The does not support this function. Pulse MeasurementOff - Source and Receivers are NOT pulsed Standard Pulse - With pulsed RF, the VNA can be configured to sweep in frequency, power sweep, and CW time. Pulse TimingRF Pulse Width - Sets the width of the RF Source pulse. Pulse Period (menu) - Allows the selection of the following:
Labels:
Pulse DetailsGenerator - Pulse generator outputs in numerical order. Device - Indicates the device being controlled by the pulse generator output.
Width - RF Source pulse width. This setting is the same as Pulse Width under RF Pulse. Delay - If the Offset Pulses using ADC Delay check box is disabled, then the delays are the pulse delays relative to the trigger. If the Offset Pulses using ADC Delay check box is enabled, then the delays are defined for the pulses relative to each other. In this case, you can enter negative delays, and the delay from the trigger will be adjusted to correct for these values. Invert - Check to cause the pulse ON time to be active low and OFF be active high. Enable Check to enable individual pulse generators. Autoselect Receiver Timing - Computes the width to 80% of the RF Source Width and the delay will be 10% of the RF Source Width. With this setting selected, the Width and Delay columns in the table are grayed out. Offset Pulses using ADC Delay Check Box
Timing Example Assume Pulse1 is used to modulate the RF signal, all Pulse outputs are enabled, all are set to zero delay, and all are set to the same width. The first timing diagram below is with offset off and the second timing diagram is with offset on.
Pulse Generators... (button)This button is only available if Pulse is enabled. Opens the Pulse Generators Setup dialog. Plot Pulse Timing... (button)This button is only available if Pulse is enabled. Accesses the Pulse Timing dialog with an interactive screen, displaying pulse characteristics in the time domain. Plot Pulse is disabled for all narrowband pulse measurements. This dialog is accessed from both the Pulse Setup and Pulse Generators Setup dialogs. Right-click on the display area to access the menu selections described below:
Autoscale - Automatically scales the data to fit vertically within the display grid area. Display marker annotation - Select to display marker annotation in the top-right of the display. Show graticule - Select to display the graticule. Add marker to: - Select to add a marker to a displayed pulse trace. When a selection is made, the mouse pointer changes to a "+". Click in the display area and the marker will appear. Drag the marker to the desired position. Each time this selection is made, a new marker will be added. Copy to Clipboard - Copies a bitmap of the trace control (Display) to the clipboard. It can then be pasted into any document that accepts bitmaps. Print... - Prints the displayed data. Scale properties... - Accesses the Scale Properties dialog: Stimulus - Sets the Begin and End displayed on the X-axis in seconds. Response - Sets the Reference level in the center of the Y-axis and sets the scale per division.
|
Pulse Generators Setup Dialog (PNA/PNA-X)
Pulse Generators Setup Dialog (PNA-X Pro)
This dialog is available with Option S9x025A/B and S9x024B (pulse generators). To see this dialog, click Pulse Generators... in the Pulse Setup dialog. Pulse Generators (table)Configure the Pulse Generators to be used for your measurement. The pulse 0 is for the receiver. The pulse 1 is for source and P1 output and pulse 2 to 4 are for P2 to P4 output signal, respectively.
Important: If D + W is greater than P, then undefined VNA behavior results. There is NO error message or warning. Learn more about the Pulse Generators. InvertCheck to cause the pulse ON time to be active low and OFF be active high. EnableCheck to enable individual pulse generators. Trigger (combo box)All trigger fields are coupled. Changing one changes all. The internal Pulse Generators can NOT be triggered individually. This provides the same selections as provided in the Pulse Setup dialog and the Trigger dialog on its "Pulse Trigger" tab.
This combo box allows you to select the pulse trigger source. Choices include the following:
FrequencySet the pulse frequency of all pulse generators.
PeriodSet the period of all pulse generators. Pulsed Sources (table)For NA520xA PNA-X Pro models, pulse sources are available with pulse modulation hardware Options PM1, PM2, PM3, PM4. Check to enable the required internal source ports. These are switches 8 and 9 in the Block Diagram. Important: When internally modulating the sources, source leveling is automatically set to Open-loop (ALC Open Loop box will be checked automatically). Shows either two or four sources depending on the hardware. The source row labels, are not affected by the simultaneous Source license. Enable (checkbox)Enables source modulation. Disabled by default. The Enable checkboxes are not affected by the simultaneous Source license. Modulation (combo box)Choose the pulse generator to modulate the specified source. Choose from CW (no pulse), Pulse 1, 2, 3, 4 and so on..., External. This is switch 7 in the Block Diagram. If the VNA option does not allow pulse on a given source, then it is grayed-out. The Modulation choices are not affected by the simultaneous Source license. ALC Hardware (combo box)There are two choices: Open Loop and Internal. Default = Open Loop This is equivalent to the softkey selection Power > Leveling & Offsets > ALC Hardware. This replaces the legacy selection "ALC Open Loop." If option does not allow pulse on a given source, then this combo box is still available. The source ALC Hardware choices are not affected by the simultaneous Source license. PropertiesSynchronize ADCs using Pulse TriggerCheck to enable triggering used to gate the ADC for wideband receiver measurements. This is the same as Pulse0 Enable The Width cannot be configured. Pulse4 Output IndicatesCheck to use an oscilloscope connected to the pulse 4 (pin 13 of the PULSE I/O connector on the rear panel of the VNA) to display when the ADC is making measurements. There are two selections:
Offset Pulse Delays Using (checkbox)This checkbox is also found in the Pulse Setup dialog. Disabled by default. When enabled, the Nominal RF Mode Delay and Rcvr ADC Delay may be subtracted from the delay values displayed. The delay terms compensated for in this subtraction depends on the position of the element in the signal processing chain that this pulse generator is driving. For example, pulse generators driving modulators have no delay subtracted, but a pulse generator driving ADC triggering (Pulse0) will have the Nominal RF Mode Delay and Rcvr ADC Delay subtracted from its delay. Modulator DelayThis is the approximate delay of the RF modulator. This value is always active and may be changed as needed. If "Auto Width and Delay" is enabled, this will be used to automatically set the delay. If "Offset Pulse Delays Using" is enabled, this will be used to offset the delay values in the table. In Narrowband Detection mode, this value is used to offset the X-axis timing. ADC Delay(Not shown on NA520xA PNA-X Pro models.) This is the delay of the receiver ADCs. This value is fixed and cannot be changed. If "Auto Width and Delay" is enabled, this will be used to automatically set the delay. If "Offset Pulse Delays Using" is enabled, this will be used to offset the delay values in the table. In Narrowband Detection mode, this value is used to offset the X-axis timing of pulse profile measurements. Offset Pulse ExampleAssume Pulse1 is used to modulate the RF signal, all Pulse outputs are enabled, all are set to zero delay, and all are set to the same width. The first timing diagram below is with offsets off and the second timing diagram is with offsets on.
Trigger... (button)Accesses the Trigger dialog on the Pulse Trigger tab. Plot Pulse... (button)This button is only available if Pulse is enabled. Accesses the Pulse Timing dialog with an interactive screen, displaying pulse characteristics in the time domain. Plot Pulse is disabled for all narrowband pulse measurements. This dialog is accessed from both the Pulse Setup and Pulse Generators Setup dialogs. Right-click on the display area to access the menu selections described below:
Autoscale - Automatically scales the data to fit vertically within the display grid area. Display marker annotation - Select to display marker annotation in the top-right of the display. Show graticule - Select to display the graticule. Add marker to: - Select to add a marker to a displayed pulse trace. When a selection is made, the mouse pointer changes to a "+". Click in the display area and the marker will appear. Drag the marker to the desired position. Each time this selection is made, a new marker will be added. Copy to Clipboard - Copies a bitmap of the trace control (Display) to the clipboard. It can then be pasted into any document that accepts bitmaps. Print... - Prints the displayed data. Scale properties... - Accesses the Scale Properties dialog: Stimulus - Sets the Begin and End displayed on the X-axis in seconds. Response - Sets the Reference level in the center of the Y-axis and sets the scale per division.
|
|
To see this dialog, press Pulse Trigger on the Pulse Generator Setup dialog or select Stimulus, then Trigger from the VNA Menu. Trigger SourceSelect Internal or External to provide sync capability for the internal pulse generators.
Trigger Level/EdgeSets the edge or level of the trigger signal to which the internal pulse generators will respond when being externally triggered at the PulseSyncIn pin.. Positive = rising edge; Negative = falling edge. These selections are available ONLY with DSP version: 4.0 FPGA: 34 or higher. Learn more. Otherwise, the pulse generators respond only to positive, level input trigger signals. Receiver synchronizationSynchronize ADCs using pulse trigger - Check to enable triggering used to gate the ADC for wideband receiver measurements. The Width can NOT be configured. ADC trigger delay - Set the amount of time to wait before triggering the ADC to begin acquisition. |

See complete description at IF Path Configuration
See also Using External Pulse Generators
Using External Pulse Generators
Setup the External Pulse Generator as an External Device.
To perform a calibration in pulse mode, first configure and apply the pulse parameters (PRF, Pulse Width, Delays, IF gating, and so forth) before calibrating the system. This will ensure the VNA is configured properly during the calibration and measurement.