Write/Read |
About Pulse Measurements |
Description |
In Narrowband pulse mode, choose to set the pulse generator used to drive the source modulation automatically or manually. |
VB Syntax |
pulseMeas.AutoSelectPulseGen = bool |
Variable |
(Type) - Description |
|
pulseMeas |
A PulseMeasurementControl (object) |
|
bool |
False - Manually set source modulation drive for the measurement. True - Automatically set source modulation drive for the measurement. |
Return Type |
Boolean |
Default |
True |
Examples |
pulse.AutoSelectPulseGen = True 'Write |
|
value = pulse.AutoSelectPulseGen 'Read |
|
C++ Syntax |
HRESULT get_AutoSelectPulseGen(VARIANT_BOOL *pVal); HRESULT put_AutoSelectPulseGen(VARIANT_BOOL newVal); |
Interface |
IPulseMeasurementControl |