Read-only |
About Balanced Measurements |
Description |
Returns the positive balanced port number in the balanced DUT topology. Use SetBPort Method to set the single balanced port DUT topology. |
VB Syntax |
var = balTopology.B_BalPortPositive |
Variable |
(Type) - Description |
|
balTopology |
A BalancedTopology (object) |
|
var |
(Long Integer) Variable to store the returned value. |
Return Type |
Long Integer |
Default |
Not Applicable |
Examples |
variable = balTopology.B_BalPortPositive 'Read |
C++ Syntax |
HRESULT get_B_BalPortPositive(long *PosPort) |
Interface |
IBalancedTopology3 |