Write/Read |
About SweptIMDCal |
Description |
Sets and returns the method by which the match-correction portion of an IMD calibration is performed. Learn more. |
VB Syntax |
imd.CalMethod = value |
Variable |
(Type) - Description |
|
imd |
A SweptIMDCal (object) |
|
value |
(Enum as NAIMDCalMethod) Choose from: 0 - naIMDMatchCorrectedResponse -Performs a full 2-port cal for full match-correction. 1 - naIMDResponseOnly - Performs only a response cal instead of a full 2-port cal. |
Return Type |
Enum |
Default |
0 - naIMDMatchCorrectedResponse |
Examples |
imd.CalMethod = naIMDMatchCorrectedResponse 'Write |
|
calMeth = imd.CalMethod 'Read |
|
C++ Syntax |
HRESULT get_CalMethod(tagNAIMDCalMethod * Val) HRESULT put_CalMethod(tagNAIMDCalMethod newVal) |
Interface |
ISweptIMD |