Sets properties that are unique to a Swept IMD Cal (opt S93087A/B).
Use the Guided Calibration commands for the remaining commands to perform a Swept IMD Cal
Dim app as AgilentPNA835x.Application Set IMDcal = pna.GetCalmanager.CreateCustomCalEx(channelNum) Set IMDCalExtension = IMDcal.CustomCalConfiguration IMDCalExtension.PowerLevel = 5 |
Example Program Create and Cal a Swept IMD Measurement
Method |
InterfaceSee History |
Description |
|---|---|---|
None |
|
|
Property |
Interface |
Description |
ISweptIMDCal |
Perform the source power cal at the center frequencies or at all main tone frequencies. |
|
ISweptIMDCal |
Sets the method by which the match-correction portion of an IMD cal is performed |
|
ISweptIMDCal2 |
Enable or disable an LO power cal with an IMDx calibration. |
|
ISweptIMDCal |
Include the second order products in the calibration. |
|
ISweptIMDCal |
Sets and returns the maximum intermod product frequencies to be calibrated. |
|
ISweptIMDCal |
Set and read the power level of the source power cal. |
|
ISweptIMDCal |
Set and read the cal kit to be used for port 1 adapter compensation. |
|
ISweptIMDCal |
Superseded Use GuidedCal.PowerSensorConnectorType |
Interface |
Introduced with VNA Rev: |
ISweptIMDCal |
8.33 |
ISweptIMDCal2 |
8.55 |