Read-only |
About Source Power Cal |
Description |
This command is replaced with chan.TestPortPower. Returns the RF power level for the channel. |
VB Syntax |
value = powerCalibrator.CalPower (chan, sourcePort) |
Variable |
(Type) - Description |
|
value |
(double) - Variable to store the returned Cal power value in dBm. |
|
powerCalibrator |
(object) - A SourcePowerCalibrator object |
|
chan |
(long integer) - Channel number of the VNA. |
|
sourcePort |
(long integer) - Source port number. Use GetPortNumber to return the port number of a source that only has a string name, such as an External Source. |
Return Type |
None |
Default |
Not applicable |
Examples |
Set powerCalibrator = pna.SourcePowerCalibrator power = powerCalibrator.CalPower(1,2) 'Read |
C++ Syntax |
HRESULT get_CalPower(long channel, long sourcePort, double *pVal); |
Interface |
ISourcePowerCalibrator |