Write/Read |
About SweptIMDCal |
Description |
Sets and returns the whether to perform the source power cal at the center frequencies midway between the main tones, or at all main tone frequencies. |
VB Syntax |
imd.CalibrationFrequencies = value |
Variable |
(Type) - Description |
|
imd |
A SweptIMDCal (object) |
|
value |
(Enum as NAIMDCalibrationFrequencies) Choose from: 0 - naIMDCenterFrequencies -Perform source power calibration at only the center frequencies midway between the main tones. 1 - naIMDALLFrequencies - Perform source power calibration at all main tone frequencies. |
Return Type |
Enum |
Default |
0 - naIMDCenterFrequencies |
Examples |
imd.CalibrationFrequencies = naIMDALLFrequencies 'Write |
|
calFreq = imd.CalibrationFrequencies 'Read |
|
C++ Syntax |
HRESULT get_CalibrationFrequencies(tagNAIMDCalibrationFrequencies * Val) HRESULT put_CalibrationFrequencies(tagNAIMDCalibrationFrequencies newVal) |
Interface |
ISweptIMD |