Write / Read |
About Frequency Settings |
Description |
Sets and reads the center frequency step size of the analyzer. This command sets the manual step size (only valid when CenterFrequencyStepSizeMode is FALSE.
|
VB Syntax |
chan.CenterFrequencyStepSize = value |
Variable |
(Type) - Description |
|
chan |
(object) - A Channel object |
|
value |
(Double) - Choose a value (in Hz.) below the stop frequency of the analyzer. |
Return Type |
Double |
Default |
Default is 40 MHz. When CenterFrequencyStepSizeMode is TRUE, this value is ignored. |
Examples |
chan.CenterFrequencyStepSize = 1e5 'Write |
C++ Syntax |
HRESULT get_CenterFrequencyStepSize(Double* pVal); HRESULT put_CenterFrequencyStepSize(Double pVal); |
Interface |
IChannel25 |