Frequency Range


Frequency range is the span of frequencies you specify for making a device measurement.

See other 'Setup Measurements' topics

How to set Frequency Range

You can also make these settings and more from the Sweep Type dialog.

See the frequency ranges of all analyzer models.

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Freq> Main > Start, Stop, Center, or  Span.

  2. Enter desired frequency value.

  1. Right click on the X-axis label or stimulus range area under grid line.

  2. Click on Start/Stop/Center....

 

Frequency Start/Stop - Center/Span - Step dialog box help

Programming Commands

Either of the following pairs of settings determine the frequency range. The last value that you enter determines the X-Axis labels. For example, if you enter the Start and Span values, the X-Axis will show Center and Span labels.

Start /Stop - Specifies the beginning and end frequency of the swept measurement range.

Note: The start frequency at preset may not be the minimum value in full range.

Center /Span - Specifies the value at the center and frequency range.

Either of the following settings determine the number of evenly-spaced data points across the frequency range.

Points - Specifies the number of evenly-spaced data points across the frequency range. Learn more about Data Points.

Step - Available ONLY in Linear sweep type. Specifies the frequency step size between evenly-spaced data points. Changes to this setting will cause the Points setting to adjust to the closest integer. Any 'remainder' will adjust either the Stop value or Span value depending on which is displayed on the X-Axis label.

Zoom

Zoom allows you to easily change the start and stop frequencies or start and stop power levels in a power sweep.

Zoom operates on the Active Trace and all traces in the same channel as the active trace, regardless of the window in which they appear.

How to Zoom in a measurement window

  1. Left-click the mouse or use a finger, then drag across a portion of a trace.

  2. Release the mouse or lift the finger and the following menu appears:

  3. Select from the following:

  • Zoom - changes the channel stimulus settings to the left and right border values of the Zoom selection

  • Zoom xy - changes the channel stimulus settings as above. In addition, the Y-axis scale of the active trace changes to the approximate scale of the Zoom selection.

  • Zoom Full Out - changes the channel stimulus settings to the full span of the current calibration. If no calibration is ON, then the stimulus settings are changed to the full span of the VNA model.

Notes

  • The stimulus settings are changed for ALL traces in the active channel, regardless of the window in which they appear.

  • If markers are in the selected area, they remain in place.

  • If markers are in the unselected area, they are moved to the right or left edge of the new span. When Zoom Full Out is selected, the markers are moved back to their original location.

Zoom is NOT available for the following:

CW Frequencies

Measurements with a CW Time sweep or Power sweep are made at a single frequency rather than over a range of frequencies.

How to set CW Frequency

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Set Sweep Type to CW Time or Power Sweep.

  2. Press Freq > Main > CW.

  3. Enter desired CW frequency.
  1. Set Sweep Type to CW Time or Power Sweep.

  2. Right click on the stimulus range area under grid box.

  3. Click on CW....

Programming Commands

 

CW Frequency dialog box help

CW  Type a value and the first letter of the suffix (k,m,or g) or use the up and down arrows to select any value within the range of the VNA.

Frequency Resolution

The resolution for setting frequency is 1 Hz.

Frequency Band Crossings

The frequency range of the VNA covers several internal frequency bands. The higher the frequency range of the VNA, the larger the number of bands. The source power to your DUT turns off as the stimulus frequency is swept through these band crossings. To learn more, see Power ON and OFF during Sweep and Retrace.

The listed frequencies in the following tables are the stop frequency of the specified band, and the start frequency of the following band.

You can download a VNA Band Structure Readout utility that lists the band crossings for your VNA.

Frequency band crossings are different for the following models:

PNA-X Models Band Stop Frequencies (with synthesizer revision greater than 6)

N5241B and N5242B

Band

Freq (GHz)

Band

Freq (GHz)

Band

Freq (GHz)

 

0

Reserved

12

.396

24

12.00

 

1

.010

13

.500

25

12.80

 

2

.014

14

.628

26

13.51

 

3

.019

15

1.00

27

15.20

 

4

.027

16

1.50

28

16.00

 

5

.038

17

2.00

29

18.00

 

6

.053

18

3.20

30

19.04

 

7

.075

19

5.332

31

20.00

 

8

.105

20

6.00

32

21.30

 

9

.146

21

7.6

33

24.00

 

10

.205

22

8.5

34

26.50

 

11

.250

23

9.52

   

 

 

 

 

 

   

 

 

N5244B and N5245B

Band

Freq (GHz)

Band

Freq (GHz)

Band

Freq (GHz)

Band

Freq (GHz)

0

Reserved

12

.396

24

12.00

36

30.40

1

.010

13

.500

25

12.80

37

32.00

2

.014

14

.628

26

13.51

38

36.10

3

.019

15

1.00

27

15.20

39

38.08

4

.027

16

1.50

28

16.00

40

40.53

5

.038

17

2.00

29

19.04

41

42.00

6

.053

18

3.20

30

20.00

42

43.50

7

.075

19

5.332

31

21.30

43

45.60

8

.105

20

6.00

32

24.00

44

48.00

9

.146

21

7.60

33

26.50

45

50.00

10

.205

22

8.50

34

27.02

 

 

11

.250

23

9.52

35

28.50

 

 

 

N5247B

Band

Freq (GHz)

Band

Freq (GHz)

Band

Freq (GHz)

Band

Freq (GHz)

Band

Freq (GHz)

0

Reserved

12

.396

24

12.00

36

30.40

48

60.10

1

.010

13

.500

25

12.80

37

32.00

49

60.80

2

.014

14

.628

26

13.51

38

36.10

50

64.00

3

.019

15

1.00

27

15.20

39

38.08

51

66.80

4

.027

16

1.50

28

16.00

40

40.00

52

70.00

5

.038

17

2.00

29

19.04

41

40.53

 

 

6

.053

18

3.20

30

20.00

42

45.82

 

 

7

.075

19

5.332

31

21.30

43

48.00

 

 

8

.105

20

6.00

32

24.00

44

50.00

 

 

9

.146

21

7.60

33

26.50

45

53.00

 

 

10

.205

22

8.50

34

27.02

46

54.04

 

 

11

.250

23

9.52

35

28.50

47

57.30

 

 

 

PNA-X Models Band Stop Frequencies (with synthesizer revision 6 or earlier)

N5241B and N5242B

Band

Freq (GHz)

Band

Freq (GHz)

Band

Freq (GHz)

 

0

Reserved

12

.396

24

8.50

 

1

Reserved

13

.500

25

10.664

 

2

.014

14

.628

26

12.00

 

3

.019

15

1.00

27

12.80

 

4

.027

16

1.50

28

13.51

 

5

.038

17

2.00

29

15.40

 

6

.053

18

3.00

30

16.00

 

7

.075

19

3.20

31

18.00

 

8

.105

20

4.00

32

20.00

 

9

.146

21

5.332

33

21.328

 

10

.205

22

6.752

34

22.50

 

11

.250

23

8.00

35

24.00

 

 

 

 

 

36

27.00

 

 

N5244B and N5245B

Band

Freq (GHz)

Band

Freq (GHz)

Band

Freq (GHz)

Band

Freq (GHz)

 

0

Reserved

12

.396

24

8.50

36

27.008

 

1

Reserved

13

.500

25

10.664

37

32.00

 

2

.014

14

.628

26

12.00

38

36.50

 

3

.019

15

1.00

27

12.80

39

40.50

 

4

.027

16

1.50

28

13.51

40

42.656

 

5

.038

17

2.00

29

15.40

41

43.50

 

6

.053

18

3.00

30

16.00

42

46.20

 

7

.075

19

3.20

31

19.00

43

48.00

 

8

.105

20

4.00

32

20.00

44

50.20

 

9

.146

21

5.332

33

21.328

 

 

 

10

.205

22

6.752

34

24.00

 

 

 

11

.250

23

8.00

35

26.50

 

 

 

 

N5247B

Band

Freq (GHz)

Band

Freq (GHz)

Band

Freq (GHz)

0

Reserved

12

6.75

24

32.00

1

Reserved

13

8.00

25

40.00

2

.053

14

10.70

26

40.50

3

.175

15

13.50

27

42.70

4

.250

16

15.40

28

46.20

5

.500

17

16.00

29

48.00

6

1.000

18

19.00

30

50.00

7

2.000

19

20.00

31

54.00

8

3.000

20

21.30

32

60.00

9

3.200

21

24.00

33

64.00

10

4.000

22

26.50

34

67.00

11

5.330

23

27.00

35

70.00

N522xB Models Band Stop Frequencies (with synthesizer revision greater than 6)

N5221B and N5222B

Band

Freq (GHz)

Band

Freq (GHz)

0

Reserved

12

15.20

1

.010

13

16.00

2

.053

14

18.00

3

.175

15

19.04

4

.250

16

20.00

5

.500

17

21.30

6

3.20

18

24.00

7

6.00

19

26.50

8

7.60

   

9

9.52

   

10

12.00

   

11

13.51

   

 

N5224B and N5225B

Band

Freq (GHz)

Band

Freq (GHz)

Band

Freq (GHz)

0

Reserved

12

15.20

24

38.08

1

.010

13

16.00

25

40.53

2

.053

14

19.04

26

42.00

3

.175

15

20.00

27

43.50

4

.250

16

21.30

28

45.60

5

.500

17

24.00

29

48.00

6

3.20

18

26.50

30

50.00

7

6.00

19

27.02

 

 

8

7.60

20

28.50

 

 

9

9.52

21

30.40

 

 

10

12.00

22

32.00

 

 

11

13.51

23

36.10

 

 

 

N5227B

Band

Freq (GHz)

Band

Freq (GHz)

Band

Freq (GHz)

Band

Freq (GHz)

0

Reserved

12

15.20

24

38.08

36

66.80

1

.010

13

16.00

25

40.00

37

70.00

2

.053

14

19.04

26

40.53

 

 

3

.175

15

20.00

27

45.82

 

 

4

.250

16

21.30

28

48.00

 

 

5

.500

17

24.00

29

50.00

 

 

6

3.20

18

26.50

30

53.00

 

 

7

6.00

19

27.02

31

54.04

 

 

8

7.60

20

28.50

32

57.30

 

 

9

9.52

21

30.40

33

60.10

 

 

10

12.00

22

32.00

34

60.80

 

 

11

13.51

23

36.10

35

64.00

 

 

N522xB Models Band Stop Frequencies (with synthesizer revision 6 or earlier)

N5221B and N5222B

Band

Freq (GHz)

Band

Freq (GHz)

0

Reserved

12

6.752

1

.010

13

8.0

2

.053

14

10.664

3

.175

15

13.51

4

.250

16

15.40

5

.500

17

16.0

6

1.0

18

20.0

7

2.0

19

21.328

8

3.0

20

24.0

9

3.2

21

27.0

10

4.0

22

 

11

5.332

23

 

 

N5224B and N5225B

Band

Freq (GHz)

Band

Freq (GHz)

Band

Freq (GHz)

0

Reserved

12

6.752

24

32.00

1

Reserved

13

8.00

25

40.50

2

.053

14

10.664

26

42.656

3

.175

15

13.51

27

43.50

4

.250

16

15.40

28

46.20

5

.500

17

16.00

29

48.00

6

1.000

18

19.00

30

50.20

7

2.000

19

20.00

 

 

8

3.000

20

21.328

 

 

9

3.200

21

24.00

 

 

10

4.000

22

26.50

 

 

11

5.332

23

27.008

 

 

 

N5227B

Band

Freq (GHz)

Band

Freq (GHz)

Band

Freq (GHz)

0

Reserved

12

6.752

24

32.00

1

.010

13

8.00

25

40.00

2

.053

14

10.664

26

40.50

3

.175

15

13.51

27

42.656

4

.250

16

15.40

28

46.20

5

.500

17

16.00

29

48.00

6

1.000

18

19.00

30

50.00

7

2.000

19

20.00

31

54.00

8

3.000

20

21.328

32

60.00

9

3.200

21

24.00

33

64.00

10

4.000

22

26.50

34

67.00

11

5.332

23

27.008

35

70.00

N523xModels  See N523x Freq ranges.

N5231B, N5232B, N5239B

Band

Freq (GHz)

Band

Freq (GHz)

0

Reserved

10

5.33

1

.000425

11

6.75

2

.0012

12

8.00

3

.0075

13

10.07

4

.025

14

13.50

5

.050

15

16.00

6

1.00

16

16.70

7

2.00

17

20.01

8

3.00

 

 

9

4.00

 

 

N5234B, N5235B Models

Band

Freq (GHz)

Band

Freq (GHz)

Band

Freq (GHz)

0

 

11

10.66

21

30.80

1

.010

12

13.51

22

31.50

2

.250

13

15.40

23

32.00

3

.500

14

16.00

24

40.00

4

1.00

15

20.00

25

40.56

5

2.00

16

20.26

26

42.00

6

3.00

17

21.33

27

48.00

7

4.00

18

24.00

28

50.00

8

5.332

19

26.00

 

 

9

6.752

20

27.01

 

 

10

8.00

 

 

 

 

Auto Tune

The Auto Tune softkey is a feature of the Spectrum Analyzer measurement class (Option S9x09xxA/B, S9x090A/B). Each time this softkey is pressed, all defined distortion measurement bands for the modulation channel are automatically tuned.

Span All Meas Bands

The Span All Meas Bands softkey is a feature of the Modulation Distortion measurement class (Option S93070xB, S9x070A/B only). Each time this softkey is pressed, all defined distortion measurement bands for the modulation channel are automatically tuned.