Write/Read |
About Swept IMD |
Description |
Sets and returns the method by which CTB and CSO calculations are performed. |
VB Syntax |
imd.CompositeNormalizationMode = value |
Variable |
(Type) - Description |
|
imd |
A SweptIMD Object |
|
value |
(Enum) 0 - naNone - the normalized power is not used in calculation 1 - naNumberOfCarriers - CTB and CSO is corrected by subtracting 10*log(N/2), where
2 - naPdBm - the composited normalized power for CTB or CSO is treated as a dBm value 3 - naPdBmV - the composited normalized power for CTB or CSO is treated as a dBmV value. Note: Power values are stored using the currently-set units. Therefore, first set units with this command, then set power values using: |
Return Type |
Enum |
Default |
naNumberOfCarriers |
Examples |
imd.CompositeNormalizationMode = naNone 'Write |
|
value = imd.CompositeNormalizationMode 'Read |
|
C++ Syntax |
HRESULT get_CompositeNormalizationMode(tagNAIMDCompositeNormalizationMode *pVal) HRESULT put_CompositeNormalizationMode(tagNAIMDCompositeNormalizationMode pVal) |
Interface |
ISweptIMD |