Write/Read |
About Swept IMD |
Description |
Sets and returns the CSO Power. Valid only with measurement parameters: CTBLo and CTBHi and for Normalization Modes dBm and dBmV. |
VB Syntax |
imd.CompositeNormalizedCTBPower = value |
Variable |
(Type) - Description |
|
imd |
A SweptIMD Object |
|
value |
(Double) Power level. The units are determined by CompositeNormalizationMode Property, which must be set first. |
Return Type |
Double |
Default |
0 |
Examples |
imd.CompositeNormalizedCTBPower = -5 'Write |
|
value = imd.CompositeNormalizedCTBPower 'Read |
|
C++ Syntax |
HRESULT get_CompositeNormalizedCTBPower(double *pVal) |
Interface |
ISweptIMD |