Write/Read |
About Coupled Markers |
Description |
Sets and Reads the scope Coupled Markers. Note: This command will not take effect until CoupledMarkers Property is turned on. Note: The preset behavior of Coupled Markers depends on the setting of MarkCoupControlsMkrState, MarkCoupMethPresetIsChan, and MarkCoupPresetIsOn. |
VB Syntax |
app.CoupledMarkersMethod = value |
Variable |
(Type) - Description |
|
app |
An Application (object) |
|
value |
(Enum as NAMarkerCouplingMethod) 0 - naMarkerCouplingAll - Coupling occurs across all channels. 1 - naMarkerCouplingChannel - Coupling is limited to traces in the same channel. |
Return Type |
Enum |
Default |
0 - naMarkerCouplingAll |
Examples |
app.CoupledMarkersMethod = naMarkerCouplingAll 'Write |
|
coupl = app.CoupledMarkersMethod 'Read |
|
C++ Syntax |
HRESULT put_CoupledMarkersMethod(tagNAMarkerCouplingMethod, value) HRESULT get_CoupledMarkersMethod(NAMarkerCouplingMethod, *value) |
Interface |
IApplication20 |