Write/Read |
About Time Domain Trace Coupling |
Description |
Specifies the time domain gating parameters to be coupled. The settings for those parameters will be copied from the active measurement to all other measurements on the channel. To turn coupling ON and OFF, use CoupleChannelParams Property To specify Transform parameters to couple, use Transform.CoupledParameters Property |
VB Syntax |
gate.CoupledParameters = value |
Variable |
(Type) - Description |
|
trans |
A Gating (object) |
|
value |
(Enum As NAGatingCoupledParams) - Parameters to couple. To specify more than one parameter, add the numbers. Choose from: 1 - naGatingStimulusCoupled (Start, Stop, Center, and Span TIME settings.) 2 - naGateStateCoupled (ON / OFF) 4 - naGatingShapeCoupled (Minimum, Normal, Wide, and Maximum) 8 - naGatingTypeCoupled (Bandpass and Notch) |
Return Type |
Enum |
Default |
29 |
Examples |
gate.CoupledParameters = 15 'Couple all parameters |
|
CP = gate.CoupledParameters 'Read |
|
C++ Syntax |
HRESULT get_CoupledParameters(long *lParams); HRESULT put_CoupledParameters(long lParams); |
Interface |
IGating2 |