Write/Read |
About Time Domain Trace Coupling |
Description |
Specifies the time domain transform parameters to be coupled. The settings for those parameters will be copied from the active measurement to all other measurements on the channel. To turn coupling ON and OFF, use CoupleChannelParams Property To specify Gating parameters to couple, use Gate.CoupledParameters Property |
VB Syntax |
trans.CoupledParameters = value |
Variable |
(Type) - Description |
|
trans |
A Transform (object) |
|
value |
(Enum As NATransformCoupledParams) - Parameters to couple. To specify more than one parameter, add the numbers. Choose from: 1 - naTransformStimulusCoupled (Start, Stop, Center, and Span TIME settings.) 2 - naTransformStateCoupled (ON / OFF) 4 - naTransformWindowCoupled (Kaiser Beta / Impulse Width) 8 - naTransformModeCoupled (Low Pass Impulse, Low Pass Step, Band Pass) 16 - naTransformDistMkrUnitCoupled (Distance maker Units) |
Return Type |
Enum |
Default |
29 |
Examples |
trans.CoupledParameters = 31 'Couple all parameters |
|
CP = trans.CoupledParameters 'Read |
|
C++ Syntax |
HRESULT get_CoupledParameters(long *lParams); HRESULT put_CoupledParameters(long lParams); |
Interface |
ITransform2 |