Read-only |
About SA Application |
Description |
Returns the byte size of the data to be exported in binary mode. Note: Returned number can exceed the maximum integer number size. In that case, an error will be raised. For that reason, we provide an access to larger numbers with the same query and LSB or MSB suffixes. |
VB Syntax |
value = sa.dft.DataByteSize |
Variable |
(Type) - Description |
|
sa.dft |
A SpectrumAnalyzerDFT (object) |
|
value |
(Variant) Variable to store the returned value. |
Return Type |
Variant |
|
Example |
value = sa.dft.DataByteSize 'Read |
C++ Syntax |
HRESULT get_DataByteSize(VARIANT* val); |
Interface |
ISpectrumAnalyzerDFT |