Read-only |
About SA Application |
Description |
Returns the frequency of the first RF bin. Note: This value can differ slightly from the SA Sweep start frequency, the frequency of the first RF bin is aligned with the current DFT grid. |
VB Syntax |
value = sa.dft.DataFirstRFBin |
Variable |
(Type) - Description |
|
sa.dft |
A SpectrumAnalyzerDFT (object) |
|
value |
(Double) Variable to store the returned value. |
Return Type |
Double |
|
Example |
value = sa.dft.DataFirstRFBin 'Read |
C++ Syntax |
HRESULT get_DataFirstRFBin(double* val); |
Interface |
ISpectrumAnalyzerDFT |