Write/Read |
About SA Application |
Description |
Sets and returns the data format. |
VB Syntax |
sa.dft.DataFormat = value |
Variable |
(Type) - Description |
|
sa.dft |
A SpectrumAnalyzerDFT (object) |
|
value |
(enum NASADataType) - Choose from: 0 naSAFloatMAGdb: Set data format to log magnitude in dBm. 1 naSAFloatAMPVolt: Set data format to linear magnitude in volts. 2 naSAPackedInt: Set data format to Packed Integers: a more compact (2 bytes) numeric representation for dBm. Each set of 2 bytes is a short number s, to get the dBm value compute (s/200.0 -36.165). |
Return Type |
Enum as NASADataType |
Default |
naSAFloatMAGdb |
Examples |
sa.dft.DataFormat = naSAFloatMAGdb 'Write |
|
FormatType = sa.dft.DataFormat 'Read |
|
C++ Syntax |
HRESULT get_DataFormat(tagNASADataType* pVal) |
Interface |
ISpectrumAnalyzerDFT |