Write/Read |
About Distance MarkerSettings |
Description |
Specifies the unit of measure for the display of marker distance values. This settings affects the display of ALL markers for only the ACTIVE measurement (unless Distance Maker Units are coupled using CoupledParameters Property. |
VB Syntax |
trans.DistanceMarkerUnit = value |
Variable |
(Type) - Description |
|
trans |
A Transform (object) |
|
value |
(Enum As NADistanceMarkerUnit) - Distance Marker Units. Choose from 0 - naDistanceMarkerUnitMeter 1 - naDistanceMarkerUnitFeet 2 - naDistanceMarkerUnitInch |
Return Type |
Enum |
Default |
0 - naDistanceMarkerUnitMeter |
Examples |
trans.DistanceMarkerUnit = naDistanceMarkerUnitFeet 'sets the |
|
U = trans.DistanceMarkerUnit 'Read |
|
C++ Syntax |
HRESULT get_DistanceMarkerUnit(tagNADistanceMarkerUnit *pVal); HRESULT put_DistanceMarkerUnit(tagNADistanceMarkerUnit newVal); |
Interface |
ITransform2 |