Write/Read |
About Distance Markers |
Description |
Set or query marker distance on a time domain trace. The Write command moves the marker to the specified distance value. Once moved, you can read the Y axis value or read the X-axis time value. (Distance is calculated from the X-axis time value.) The Read command reads the distance of the marker. If the marker is set as delta, the WRITE and READ data is relative to the reference marker. |
VB Syntax |
mark.Distance = value |
Variable |
(Type) - Description |
|
mark |
A Marker (object) |
|
value |
(double) - Marker distance in the unit of measure specified with DistanceMarkerUnit Property |
Return Type |
Double |
Default |
Not Applicable |
Examples |
mark.Distance = 3e9 'Write |
|
XVal = mark.Distance 'Read |
|
C++ Syntax |
HRESULT get_Distance(double *pVal); HRESULT put_Distance(double newVal); |
Interface |
IMarker2 |