Write/Read |
About Dwell Time |
Description |
Sets or returns the dwell time at the start of each sweep point for all measurements in a channel. Dwell time is only available with Chan.SweepGenerationMode = naSteppedSweep (not naAnalogSweep). Sets or returns the dwell time of a specified sweep segment. |
VB Syntax |
object.DwellTime = value |
Variable |
(Type) - Description |
|
object |
A Channel (object) or CalSet (object) - Read-only property or Segment (object) |
|
value |
(double) - Dwell Time in seconds. Choose any number between 0 and 86400. Note that 0 is equivalent to no dwell time. |
Return Type |
Double |
Default |
0 |
Examples |
chan.DwellTime = 3e-3 'sets the dwell time for the channel -Write segs(3).DwellTime = 5e-3 'sets the dwell time of segment 3 -Write |
|
dwell = chan.DwellTime 'Read |
|
C++ Syntax |
HRESULT get_DwellTime(double *pVal) |
Interface |
IChannel |CalSet3 |