Read-only |
About SA Application |
Description |
Returns the currently exported receiver list. Note: The list is set with ExportReceiverSetList can contain more receivers, this query will only return the ones that are currently measured and that are in the receiver list. |
VB Syntax |
list = sa.dft.ExportReceiverList |
Variable |
(Type) - Description |
|
sa.dft |
A SpectrumAnalyzerDFT (object) |
|
list |
(String) Variable to store the returned list. |
Return Type |
String |
|
Example |
list = sa.dft.ExportReceiverList 'Read |
C++ Syntax |
HRESULT get_ExportReceiverList(BSTR* ReceiverList); |
Interface |
ISpectrumAnalyzerDFT |