Write/Read |
About SA Application |
Description |
Enables/disables erasing output data files after each sweep. When disabled, data is appended to the output file after each sweep which could lead to very large files sizes (and eventually fill the disk). |
VB Syntax |
sa.dft.FileEraseEachSweep = value |
Variable |
(Type) - Description |
|
sa.dft |
A SpectrumAnalyzerDFT (object) |
|
value |
(Boolean) Choose from: 0 - OFF - Erase data files after each sweep disabled. 1 - ON - Erase data files after each sweep enabled. |
Return Type |
Boolean |
Default |
ON |
Examples |
sa.dft.FileEraseEachSweep = ON 'Write |
|
value = sa.dft.FileEraseEachSweep 'Read |
|
C++ Syntax |
HRESULT get_FileEraseEachSweep(VARIANT_BOOL* enable) |
Interface |
ISpectrumAnalyzerDFT |