Write/Read |
About SA Application |
Description |
Sets and returns the file name prefix for the data file. The receivers selected in ExportReceiverSetList will be appended to the specified prefix name with either "_X.txt" if a text file is exported (TextFileEnabled) or "_X.bin" if a binary file is exported (BinaryFileEnabled). X is the receiver name. |
VB Syntax |
sa.dft.FilePrefix = prefix |
Variable |
(Type) - Description |
|
sa.dft |
A SpectrumAnalyzerDFT (object) |
|
prefix |
(String) Specified prefix. |
Return Type |
String |
|
Example |
sa.dft.FilePrefix = "C:\TEMP\SA_DATA_OUT" 'Write |
|
value = sa.dft.FilePrefix 'Read |
|
C++ Syntax |
HRESULT get_FilePrefix(BSTR* prefix); HRESULT put_FilePrefix(BSTR prefix); |
Interface |
ISpectrumAnalyzerDFT |