Read only |
About VNA Options |
Description |
Returns the alpha portion of the firmware revision number. For example, given a firmware revision number A.03.30, this command returns A. |
VB Syntax |
value = cap.FirmwareSeries |
Variable |
(Type) - Description |
|
value |
(String) - Variable to store the returned alpha value of the firmware revision number. |
|
cap |
A Capabilities (object) |
Return Type |
String |
Default |
Not Applicable |
Examples |
value = cap.FirmwareSeries 'Read |
C++ Syntax |
HRESULT get_FirmwareSeries(BSTR * series); |
Interface |
ICapabilities |