Write/Read |
About Frequency Range |
Description |
Sets the frequency step size across the selected frequency range. This effectively sets the number of data points. Available ONLY when SweepType = Linear. |
VB Syntax |
object.FrequencyStep = value |
Variable |
(Type) - Description |
|
object |
A Channel (object) |
|
value |
(double) - Frequency step size in Hertz. Select any value up to the frequency range of the analyzer. |
Return Type |
Double |
Default |
Not Applicable |
Examples |
chan.FrequencyStep = 1e9 'sets the frequency step size of a linear sweep for the channel object -Write |
|
freqstep = chan.FrequencyStep 'Read |
|
C++ Syntax |
HRESULT get_FrequencyStep(double *pVal) HRESULT put_FrequencyStep(double newVal) |
Interface |
IChannel24 |