Read only |
About VNA Options |
Description |
Returns the number of GPIB ports that are present on the VNA rear-panel. |
VB Syntax |
value = cap.GPIBPortCount |
Variable |
(Type) - Description |
|
value |
(Long) - Variable to store the returned integer value of the number of GPIB ports. |
|
cap |
A Capabilities (object) |
Return Type |
Long |
Default |
Not Applicable |
Examples |
value = cap.GPIBPortCount 'Read |
C++ Syntax |
HRESULT get_GPIBPortCount(long * gpibPorts ); |
Interface |
ICapabilities3 |