Read only |
About VNA Options |
Description |
Returns whether or not the analyzer has direct receiver access (front-panel jumpers). |
VB Syntax |
value = cap.HasDirectReceiverAccess |
Variable |
(Type) - Description |
|
value |
(Boolean) - Variable to store the returned value True - VNA has direct receiver access. False - VNA does NOT have direct receiver access. |
|
cap |
A Capabilities (object) |
Return Type |
Boolean |
Default |
Not Applicable |
Examples |
value = cap.HasDirectReceiverAccess 'Read |
C++ Syntax |
HRESULT get_HasDirectReceiverAccess(VARIANT_BOOL *present ); |
Interface |
ICapabilities12 |