Description |
Returns the test set ID number. For GPIB testsets, the ID is equivalent to the GPIB address. For testset I/O testsets, the ID is the base address of the testset (0 for the first testset, 1 for the second, and so on). |
VB Syntax |
value = tset.ID |
Variable |
(Type) - Description |
|
value |
(Long) variable to store the returned information. |
|
testsets(1) |
A TestsetControl object. OR An E5091Testset object. |
Return Type |
Long Integer |
Default |
Not Applicable |
Examples |
value = testset1.ID |
C++ Syntax |
HRESULT get_ID(long *idNumber); |
Interface |
ITestsetControl IE5091Testset |