Read-only |
About Source Power Cal |
Description |
Returns the pass / fail status of the tolerance limits of the target power from the most recent source power cal. |
VB Syntax |
value = pwrCal.LastCalPassedTolerance |
Variable |
(Type) - Description |
|
pwrCal |
(object) – A SourcePowerCalibrator (object) |
|
value |
(boolean) - False – Source power cal did NOT achieve the specified tolerance limits. True – Source power cal DID achieve the specified tolerance limits. |
Return Type |
Boolean |
Default |
Not Applicable |
Examples |
status = powerCal.LastCalPassedTolerance 'Read |
C++ Syntax |
HRESULT get_LastCalPassedTolerance(VARIANT_BOOL *bState); |
Interface |
ISourcePowerCalibrator7 |