Write/Read |
About Power Limit |
Description |
Sets and returns the power limit for the specified port. |
VB Syntax |
gpl.Limit (port) = value |
Variable |
(Type) - Description |
|
gpl |
A GlobalPowerLimit (object) |
|
port |
(Long) Port number for which power limit value is to be set. |
|
value |
(Double) Power limit value. Choose a value between -27 dBm (approximately) and the max settable power for the VNA. |
Return Type |
Double |
Default |
100 dBm for all ports |
Examples |
gpl.Limit(1) = 0 'Write |
|
Limit = gpl.Limit(2) 'Read |
|
C++ Syntax |
HRESULT get_Limit(long port, double *pVal) |
Interface |
IGlobalPowerLimit |