The power limit can NOT be set for power levels which are below the power level that is required by the analyzer to achieve phase lock - approximately -30 dBm.
Because Fast Sweep mode allows power spiking, it is NOT allowed when a power limit is enabled.
Components that are added to the RF path are accounted for by entering their loss (negative) or gain (positive) in the Power Offset section of the dialog box.
VNA Applications may change RF path components. For example, IMD for Converters may change the combiner path and add an amplifier for LO input. Compensation is NOT made for these changes and port power may exceed the power limit or port power may be clipped unnecessarily.
Power limiting does NOT clip power spikes that may occur during frequency band crossings.
External test set ports are also included for power limiting.
Power Offset provides a method of compensating port power for added attenuation or amplification in the source path. The result is that power at the specified port, all dialogs, and annotation, reflects the added components.
How to access the Offsets and Limits settingsAlso accessed through the Preferences dialog. |
|
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
|
Note: For NA520xA PNA-X Pro models, each port has its own unique RF source, allowing more flexibility in path configurations, such as when using combiners. Additionally, Option 2SS/4SS enables simultaneous sources, that is, the ability to turn on 2 or 4 sources at the same time. If you set a source ON and the number of simultaneous sources is exceeded, then the VNA automatically disables other sources and displays a warning in the status bar. If sources must be automatically disabled, the first sources to be disabled will be those currently in AUTO mode. The following source selections are available:
Click a WHITE cell to change values. Shaded cells can NOT be changed. Remote commands can be sent to lock and unlock the dialog box (UI) settings. Limit Source PowerLimits the source power at each test port for ALL channels. Use this feature to protect DUTs that are sensitive to overpowering at the input. Source Power levels that exceed the Limit at the specified port are clipped at the limit, the power level in the Source Power column turns red, and an error message is displayed on the screen. The Power Limit settings and PLimit status indicator survive Instrument Preset. When an Instrument State is recalled, the current Power Limit settings are applied to the recalled state. To learn more, see Power Limit Overview (scroll up). State
Limit Always - Limit the source power at all times. If Banded Power Limits are disabled for the cell, then the cell will display a fixed limit value with default value 100 dBm. Click on the cell to change the value. If Banded Power Limits are enabled, then the cell will display the text "Banded" and clicking on the cell will do nothing. Limit During Cal - Limit the source power during calibration.
Banded Power Limit
Notes: Each source has an independent set of bands, states, frequencies and power limits. Select Source Selects a source from the combo box. The default selection is the source which was chosen in the Offsets and Limits dialog. The Band Limits table is used to define the limits of the selected source. Changing to another source will display the Enable Banded Power Limits checkbox and Band Limits table for that source. User can make changes to those values. Not all External Source drivers are supported by the Power Limit feature. In particular, very old source drives with an "AG" prefix are not supported and limits cannot be set. Enable Banded Power Limits When enabled, the limits will be applied to the selected source. Default is disabled. "Row Number" of the table Each row has a number from 1 to N which is used to label the data in the saved file. State Click to toggle between two states, On or Off of the band. Default is "On". FStart, FStop Define the start and stop frequencies of the band. Default values are FStart = 0 Hz and FStop = 1 THz and the range is 0 Hz to 100 THz. Power Limit Enter the power limit value for each band by clicking on the cell. Default value is +100 dBm and the range is +/- 200 dBm with 0.01dB resolution.
Add Row Click to add a row below the last row. Remove Row Click to remove the bottow row. Save... Navigate to the directory where you want to save the Band Limits table for the selected source. The file data includes: State, Fstart, Fstop and Limit. It does not include "Select Source" and " Enable Banded Power Limits". User can copy tables between sources by saving table, changing the selected source, and then recalling the table. The file type is .csv. Recall Navigate to the directory to recall a Band Limits table for the selected source. Recall error will be shown if the selected recall file (.csv) is improperly formatted or contains invalid information. Errors found in the file will be listed in the error dialog. OK Click will close the error dialog and data in the Band Limits table will remain unchanged. OK Apply the added values in the Banded Power Limit table and close the dialog. Cancel Close the dialog without saving the added values. Apply Apply the Enable Banded Power Limits checkbox setting, frequencies and powers. If the values are changed for more than one source by using the Select Source combo box, then all new values for all sources will be applied.
Power Table Logic
Example 1 (Band Gaps):
Example 2 (Band Overlap):
For VNA models with a second internal source, the Port 1 Src2 Power Limit setting is NEVER available. Make the setting at the standard Port 1. Power OffsetPower Offset provides a method of compensating port power for added attenuation or amplification in the source path. The result is that power at the specified port, all dialogs, and annotation reflects the added components.
Important Note: Power Offset is added AUTOMATICALLY when a Source Power Calibration, Guided Power Cal, or Power Compensation is ON with Fixture Embed/Deembed. If you are NOT seeing the correct power level at your DUT, view the power Offset column in this dialog for unexpected offsets.
Optionally change the Source Power or Port Power values so that the following equation reflects your requirement: Source Power + Power Offset = Port Power Source Cal ON / OFF Notes
Power Step Size: Specify the arrow key up/down step resolution. The setting is kept even after preset and power off/on. Power Spin Size: Specify the rotary Knob spin resolution. The setting is kept even after preset and power off/on. OK Closes the dialog box.
|