Write/Read |
About Magnitude Offset |
Description |
Offsets the data trace magnitude to a value that changes linearly with frequency. The offset slope begins at 0 Hz. To offset the entire data trace magnitude by a specified value, use MagnitudeOffset Property. |
VB Syntax |
meas.MagnitudeSlopeOffset = value |
Variable |
(Type) - Description |
|
meas |
(object) - A Measurement object |
|
value |
(double) - Offset slope value in dB / 1GHz. |
Return Type |
Double |
Default |
0 |
Examples |
meas.MagnitudeSlopeOffset = 4 'Writes a slope offset of 4dB/1GHz. |
|
offs = meas.MagnitudeSlopeOffset 'Read |
|
C++ Syntax |
HRESULT put_MagnitudeSlopeOffset(double newVal); HRESULT get_MagnitudeSlopeOffset(double *pVal); |
Interface |
IMeasurement4 |