Write/Read |
About Magnitude Offset |
Description |
Offsets the data trace magnitude by the specified value. To offset the data trace magnitude to a slope value that changes with frequency, use MagnitudeSlopeOffset Property. To implement a Receiver Cal offset, use LogMagnitudeOffset property. |
VB Syntax |
meas.MagnitudeOffset = value |
Variable |
(Type) - Description |
|
meas |
(object) - A Measurement object |
|
value |
(double) - Offset value in dB. |
Return Type |
Double |
Default |
0 |
Examples |
meas.MagnitudeOffset = 4 'Write |
|
offs = meas.MagnitudeOffset 'Read |
|
C++ Syntax |
HRESULT put_MagnitudeOffset(double newVal); HRESULT get_MagnitudeOffset(double *pVal); |
Interface |
IMeasurement4 |