Write/Read |
About Marker Readout |
Description |
Specifies the size of font used when displaying Marker Readout in the selected window. |
VB Syntax |
win.MarkerReadoutSize = value |
Variable |
(Type) - Description |
|
win |
A NAWindow (object) |
|
value |
(enum NAFontSize) 0 - naDefault - marker readout appears in default font size 1 - naLarge - marker readout appears in large font size |
Return Type |
Long Integer |
Default |
naDefault |
Examples |
win.MarkerReadoutSize = naDefault 'write default size for marker readout Dim Size As NAFontSize |
C++ Syntax |
HRESULT get_MarkerReadoutSize(tagNAFontSize *pVal) HRESULT put_MarkerReadoutSize(tagNAFontSize newVal) |
Interface |
INAWindow |