Read only |
About VNA Options |
Description |
Returns the maximum possible number of windows that can be present on the VNA screen. |
VB Syntax |
value = cap.MaximumNumberOfWindows |
Variable |
(Type) - Description |
|
value |
(Long) - Variable to store the returned maximum value for number of windows. |
|
cap |
A Capabilities (object) |
Return Type |
Long |
Default |
Not Applicable |
Examples |
value = cap.MaximumNumberOfWindows 'Read |
C++ Syntax |
HRESULT get_MaximumNumberOfWindows(long * maximumNumberOfWindows ); |
Interface |
ICapabilities2 |