Read-only |
About Path Configurator |
Description |
Returns the name of the current configuration only if NO individual element settings had been changed since selecting or storing a configuration. When element settings change, the path configuration name is cleared. |
VB Syntax |
name = pathConfig.Name |
Variable |
(Type) - Description |
|
name |
(String) Variable to store the returned configuration name. |
|
pathConfig |
A PathConfiguration (object) |
Return Type |
String |
Default |
'default' - name of the default factory configuration |
Examples |
name=pathConf.Name |
C++ Syntax |
HRESULT get_Name(BSTR* ppName) |
Interface |
IPathConfiguration |