Provides access to the path configuration currently active on the channel object.
To load, store, or delete a configuration, see ConfigurationManager Object.
Dim app As AgilentPNA835x.Application
Set app = CreateObject("AgilentPNA835x.Application", <analyzerName>)
Dim chan as Channel
Set chan = app.ActiveChannel
Dim pathConfig As PathConfiguration
Set pathConfig = chan.PathConfiguration
|
Type pnaType = Type.GetTypeFromProgID("AgilentPNA835x.Application", "PNA-NAME-HERE"); AgilentPNA835x.Application pna = (AgilentPNA835x.Application)Activator.CreateInstance(pnaType); AgilentPNA835x.Channel chan = (AgilentPNA835x.Channel)pna.ActiveChannel; AgilentPNA835x.PathConfiguration path = (AgilentPNA835x.PathConfiguration)chan.get_PathConfiguration(); |
|
Note: To learn how to make configuration (element) settings, see this Path Configuration Example Also see this list of configurable elements and settings. |
Methods |
Interface |
Description |
|---|---|---|
|
IPathConfiguration2 |
Copy the mechanical switch settings and attenuator settings from the specified channel to the active channel. |
|
|
IPathConfiguration |
Saves the current configuration to the specified name. |
|
Properties |
Interface |
Description |
|
IPathConfiguration |
Write and read descriptive text associated with the configuration. |
|
|
IPathConfiguration |
Collection of Elements that can be configured (switches and so forth). See the list of elements and settings. |
|
|
IPathConfiguration |
Returns a handle to a IPathElement object. |
|
|
IPathConfiguration |
Returns the name of the current configuration. |
|
|
IPathConfiguration |
Returns a pointer to the parent COM object (Channel). |
|
Interface |
Introduced with VNA Rev: |
|
IPathConfiguration |
7.2 |
|
IPathConfiguration2 |
9.4 |