Write/Read |
About Noise Figure |
Description |
Sets and returns the noise tuner identifier, which is an ECal model and serial number string. |
VB Syntax |
noise.NoiseTuner = value |
Variable |
(Type) - Description |
|
noise |
A NoiseFigure (object) |
|
value |
(string) Noise Tuner. Return the connected ECal identifiers by sending GetCalKitTypeString and passing the module number. |
Return Type |
String |
Default |
Not Applicable |
Examples |
noise.NoiseTuner = "N4691-60004 ECal 02822"'Write |
|
noiseT = noise.NoiseTuner 'Read |
|
C++ Syntax |
HRESULT get_NoiseTuner(BSTR* pValue) HRESULT put_NoiseTuner(BSTR pNewValue) |
Interface |
INoiseFigure |