Controls the Noise Figure application settings.
|
Dim app as AgilentPNA835x.Application app.CreateCustomMeasurementEx(1, "NoiseFigure", "NF", 1) Dim NoiseFig Set NoiseFig = app.ActiveChannel.CustomChannelConfiguration |
Example programs
Method |
InterfaceSee History |
Description |
|---|---|---|
|
INoiseFigure7 |
Reads noise parameter snp data. |
|
|
INoiseFigure6 |
Maps DUT ports to PNA-X ports (Opt 028) |
|
|
INoiseFigure7 |
Reads noise parameter data to snp file. |
|
Property |
Interface |
Description |
|
INoiseFigure |
Sets the air temperature at which the measurement is being performed. |
|
|
INoiseFigure6 |
Read DUT input port map |
|
|
INoiseFigure6 |
Read DUT output port map |
|
|
INoiseFigure |
Sets the number of impedance states to use during calibrated measurements. |
|
|
INoiseFigure8 |
Enable narrowband compensation |
|
|
INoiseFigure |
Set averaging of noise receiver. |
|
|
INoiseFigure |
Turn noise averaging ON and OFF |
|
|
INoiseFigure |
Set bandwidth of noise receiver. |
|
|
INoiseFigure |
Set gain state of noise receiver. |
|
|
INoiseFigure3 |
Turns noise threshold checking ON and OFF. |
|
|
INoiseFigure5 |
Sets and returns the receiver to use for noise measurements. |
|
|
INoiseFigure3 |
Returns an estimate of sweep time. |
|
|
INoiseFigure |
Sets and returns the noise tuner identifier, |
|
|
INoiseFigure |
Sets and returns the port identifier of the ECal noise tuner Input |
|
|
INoiseFigure |
Sets and returns the port identifier of the ECal noise tuner Output |
|
|
INoiseFigure4 |
Set and read the use of source pull technique to compute S22 on Noise Figure on Converters. |
|
Interface |
Introduced with VNA Rev: |
|
INoiseFigure |
8.0 |
|
INoiseFigure3 |
9.0 |
|
INoiseFigure4 |
9.1 |
|
INoiseFigure5 |
9.2 |
|
INoiseFigure6 |
9.22 |
|
INoiseFigure7 |
9.80 |
|
INoiseFigure8 |
10.15 |