Write/Read |
About External Testset Control |
Description |
Sets or gets the port mappings for ALL ports. An “invalid argument” error will occur if you attempt to set an illegal port combination. Refer to your testset documentation for valid port combinations. Note: Do not confuse the similar E5091.OutputPort Property, which sets or gets the port mapping for a single port. |
VB Syntax |
tset.OutputPorts(chNum) = portList |
Variable |
(Type) - Description |
|
tset |
A TestsetControl object. |
|
chNum |
(Long) Channel number of the measurement. |
|
portList |
(String) A comma-separated list of port mappings. Spaces are ignored at the beginning and end of this text, and before or after commas. Space characters in other locations are not ignored. |
Return Type |
String |
Default |
Not Applicable |
Examples |
|
C++ Syntax |
HRESULT get_OutputPorts(long channelNum, BSTR *outPorts); |
Interface |
ITestsetControl |