Description |
Returns the most recent pass/fail status value. Use this command as follows:
|
VB Syntax |
var = object.PassFailStatus |
Variable |
(Type) - Description |
|
var |
(enum as NAPassFailStatus) Variable to store returned status. One of the following will be returned: 0 - naStatusFail - all measurements not in HOLD mode have been swept, and one or more limit tests failed according to the specified Pass/Fail policy. 1 - naStatusPass - all measurements not in HOLD mode have been swept, and all associated limit tests have passed. 2 - naStatusNone - status cannot be determined because measurements are in progress. |
|
object |
(object) - An Aux I/O or Handler I/O object |
Return Type |
Long Integer |
Default |
Not Applicable |
Examples |
status = aux.PassFailStatus 'Read |
C++ Syntax |
HRESULT get_PassFailPolicy ( tagNAPassFailStatus* status); |
Interface |
IHWAuxIO4 IHWMaterialHandlerIO2 |