Write/Read |
About Trigger Source |
Description |
Sets or returns the source of triggering on the VNA and PNA-X. |
VB Syntax |
trigSetup.Source = value |
Variable |
(Type) - Description |
|
trigSetup |
A TriggerSetup (object) |
|
value |
(enum NATriggerSource) - Choose from: 0 - naTriggerSourceInternal - free run 1 - naTriggerSourceManual - manual trigger source; use app.ManualTrigger to send a trigger signal. 2 - naTriggerSouceExternal - a trigger signal is generated when a signal is sensed on the appropriate external trigger input connector. Use ExternalTriggerConnectionBehavior to configure the characteristics of the external trigger signal. This setting has implications on Calibration. Learn more. |
Return Type |
Long Integer |
Default |
naTriggerSourceInternal |
Examples |
trigSetup.Source = naTriggerSourceInternal 'Write |
|
trigsource = trigSetup.Source 'Read |
|
C++ Syntax |
HRESULT get_Source(tagNATriggerSource *pTrigger); HRESULT put_Source(tagNATriggerSource trigger); |
Interface |
ITriggerSetup |