Write/Read |
About Marker Search |
Description |
Sets peak threshold for the specified marker. If a peak (using the criteria set with PeakExcursion) is below this reference value, it will not be considered when searching for peaks. |
VB Syntax |
mark.PeakThreshold = value |
Variable |
(Type) - Description |
|
mark |
A Marker (object) |
|
value |
(single) - Peak Threshold. Choose any number between: |
Return Type |
Single |
Default |
-100db |
Examples |
mark.PeakThreshold = 1 'Write |
|
PkThresh = mark.PeakThreshold 'Read |
|
C++ Syntax |
HRESULT get_PeakThreshold(float *pVal) |
Interface |
IMarker |