Read/Write |
About Guided Power Cal |
Description |
Enables Guided Power Cal and sets the source port to be calibrated. |
VB Syntax |
guidedCal.PerformPowerCalibration (port) = value |
Variable |
(Type) - Description |
|
guidedCal |
GuidedCalibration (object) |
|
port |
(Long integer) Source port to be calibrated. ONLY one port may be calibrated with a Guided Power Cal. |
|
value |
(Boolean) True Perform a Guided Power Calibration. False Do NOT perform a Guided Power Calibration |
Return Type |
Boolean |
Default |
False |
Example |
guided.PerformPowerCalibration(1) = True |
C++ Syntax |
HRESULT get_PerformPowerCalibration(long port,VARIANT_BOOL* val); HRESULT put_PerformPowerCalibration(long port,VARIANT_BOOL newVal); |
Interface |
IGuidedCalibration7 |