Read-only |
About Source Power CalAbout PMAR |
Description |
Identifies which channel of the power meter the power sensor is connected to. |
VB Syntax |
chan = powerSensor.PowerMeterChannel |
Variable |
(Type) - Description |
|
chan |
(enum NAPowerAcquisitionDevice) – Power meter channel identifier for sensor. Choose from: 0 – naPowerSensor_A 1 – naPowerSensor_B |
|
pwrSensor |
A PowerSensor (Object) or A PowerSensorAsReceiver (Object) |
Return Type |
NAPowerAcquisitionDevice |
Default |
Not Applicable |
Examples |
meterChannel = pwrSensor.PowerMeterChannel |
C++ Syntax |
HRESULT PowerMeterChannel(tagNAPowerAcquisitionDevice *pSensor); |
Interface |
IPowerSensor IPowerSensorAsReceiver |