Write/Read |
About Triggering |
Description |
Set and read the preference for the chan.Single trigger behavior. This setting persists until changed. These preferences are important when performing a Guided calibration, as the VNA uses the chan.Single trigger command to measure standards.
To set this preference for an Unguided Calibration, use PreferInternalTriggerOnUnguidedCal Property The chan.Single trigger command NEVER respects the Trigger Source = Manual setting. It always switches to Internal for one trigger, then back to Manual, regardless of this preference command. |
VB Syntax |
pref.PreferInternalTriggerOnChannelSingle = bool |
Variable |
(Type) - Description |
|
pref |
A Preferences (object) |
|
bool |
(Boolean) - Choose from: 0 - False - the Single trigger property does respect the Trigger Source = External setting. For example, if Trigger source = External, the single trigger method will wait for the External trigger signal and then allow only one sweep. 1 - True - the Single trigger command does NOT respect the Trigger Source = External setting. For example, when the Single method is sent, the VNA immediately switches to Internal sweep, responds to one trigger signal, then switches back to External. |
Return Type |
Boolean |
Default |
0 - False |
Examples |
pref.PreferInternalTriggerOnChannelSingle = False 'Write |
|
prefer = pref.PreferInternalTriggerOnChannelSingle 'Read |
|
C++ Syntax |
HRESULT put_PreferInternalTriggerOnChannelSingle( VARIANT_BOOL bprefSingle) HRESULT get_PreferInternalTriggerOnChannelSingle( VARIANT_BOOL *bprefSingle) |
Interface |
IPreferences2 |