Write/Read |
About Receiver Leveling |
Description |
Sets and returns the receiver to be used with Receiver Leveling. To perform receiver leveling with a ratioed receiver, use ReceiverRatio Property. |
VB Syntax |
RxLevel.ReferenceReceiver(srcPort) = value |
Variable |
(Type) - Description |
|
RxLevel |
A ReceiverLeveling Object |
|
srcPort |
(Long Integer) Source port for which to set the receiver for Receiver Leveling. Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port |
value |
(String) Receiver to use for the leveling sweeps. (Not case sensitive). Choose any receiver in your VNA. see the block diagram of your VNA, located at the bottom of all Specs documents. Receivers can also be referred to using logical receiver notation. This notation makes it easy to refer to receivers with an external test set connected to the VNA. You do not need to know which physical receiver is used for each test port. Learn more. |
Return Type |
String |
Default |
Not applicable |
Examples |
rxLevel.ReferenceReceiver (1) = "R1" ' Write rxLevel.ReferenceReceiver (1) = "b2" ' Write |
|
value = rxLevel.ReferenceReceiver 2' Read |
|
C++ Syntax |
HRESULT get_ReferenceReceiver( long port, BSTR* pVal); HRESULT put_ReferenceReceiver( long port, BSTR newVal); |
Interface |
IReceiverLevelingConfiguration |