Write/Read |
About SA Application |
Description |
Set and read how the resolution bandwidth is set. When ON, resolution bandwidth is set based on Span/RBW ratio. |
VB Syntax |
sa.ResolutionBWMode = value |
Variable |
(Type) - Description |
|
sa |
A SpectrumAnalyzer (object) |
|
value |
(Enum as NAModes) Choose from: 1 - naMANUAL - Res. BW is set manually using ResolutionBW Property 0 - naAUTO - Res. BW is set automatically and will not set resolution bandwidth above 300 kHz. |
Return Type |
Enum |
Default |
0 - naAUTO |
Examples |
sa.ResolutionBWMode = 1 'Write |
|
value = sa.ResolutionBWMode 'Read |
|
C++ Syntax |
HRESULT put_ResolutionBWMode(tagNAModes mode); HRESULT get_ResolutionBWMode(tagNAModes* mode); |
Interface |
ISpectrumAnalyzer |