Write/Read |
About SA Application |
Description |
Set and read the resolution bandwidth. Also set ResolutionBWMode to naManual. |
VB Syntax |
sa.ResolutionBW = value |
Variable |
(Type) - Description |
|
sa |
A SpectrumAnalyzer (object) |
|
value |
(Double) Choose a value between 6 Hz and 3 MHz. Attempting to set the bandwidth outside these bounds will force the bandwidth to the nearest bound. |
Return Type |
Double |
Default |
100 kHz |
Examples |
sa.ResolutionBW = 1e6 'Write |
|
value = sa.ResolutionBW 'Read |
|
C++ Syntax |
HRESULT put_ResolutionBW(double freq); HRESULT get_ResolutionBW(double* freq); |
Interface |
ISpectrumAnalyzer |